Manual (MB-OFDM)
Cleared (See MB-OFDM Standard Setups/Presets Table.)
(inactive Result
Length default: 108 symbol-times)
When is selected, the measurement result length is specified by the value (symbol-times) in the text box. The default is 60 symbol-times. The VSA ignores the input burst symbol length and uses the symbol length. The VSA will use this value even if it is longer than the measured signals burst length.
Manual does not limit the result length to the number of symbols transmitted within the burst as is done in the two auto modes ( and ). The VSA will demodulate the total number of symbols specified by , which if longer than the burst, could lead to unexpected and incorrect data results.
The Payload Octets can be set by entering a value in the text box. This displays the resulting Result Length (in symbols) for your particular settings of and Data Rate.
See Also
Time Tab (MB-OFDM Demod Properties)