Auto Data Rate (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Format tab

Default: Selected (See MB-OFDM Standard Setups/Presets Table.)

When the Auto Data Rate check box is selected, the VSA will automatically set the data rate to what it finds in the header. When the check box is not selected, the Data Rate is set by Format.

The Result Length and Data Rate settings determine the quantity of the Payload Octets. To learn more, see Payload Octet Calculations.

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Format Tab (MB-OFDM Demod Properties)