Max Result Length (MB-OFDM)
108 symbol-times (See MB-OFDM Standard Setups/Presets Table.)
12 symbol-times (in 6 symbol-time steps) - hardware limit
When either or in the Result Length section are selected, specifies the maximum number of symbols that can be included in the measurement result length. The VSA automatically determines the measurement result length by comparing the to the burst symbol-times in the From Pulse Search mode or to the PSDU 1) PHY Service Data Unit, or 2) PLCP SDU Length in From Header mode and using the smaller value as the measurement result length.
See Also
Time Tab (MB-OFDM Demod Properties)