Auto-detect Power Boosts (NB-IoT)
Disabled
The checkbox enables the NB-IoT demodulator to detect the power boost levels for all channels/signals (NRS, NPSS, NSSS, NPDCCH, NPDSCH, NPBCH, CRS).
-
- When enabled, the demodulator will automatically detect all of the Composite Include and Channel Configuration Power Boost settings. The settings are disabled from editing since the levels are automatically detected, and auto-detected levels will be shown in trace data.
-
- Manually set Power Boost levels in DL Down Link (forward link: from base station to cell phone) Channel Parameters dialog (Edit Control Parameters) or NPDSCH Shared Settings.
See Also