CC Summary (5G NR/5G-Advanced)

The CC Summary trace shows measurement results for each mapped carrier that is defined and enabled in the carrier aggregation panel.

CC Summary is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.

 

Not visible by default

To make visible, right-click any column heading and select Column Visibility...

               
CC Ref. CC Channel Power (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) Rel. Power (dB) EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. (%rms) TAE (sec) Center Freq. (Hz) Freq. Error(Hz) Clock Error (ppm) Cell ID

CC is name given to each carrier that is mapped in the carrier aggregation table.

Ref. CC is the CC that is specified to be the Reference in the carrier aggregation panel. The Reference CC is the reference point for the TAE cross-carrier measurement result.

Channel Power is the measurement channel power of each mapped carrier (CCx).

Rel. Power is calculated by subtracting the Channel Power of the reference CC from the Channel Power of CCx.

EVM is the per-carrier RMS EVM.

The Report EVM in dB parameter affects the units of this data result.

TAE (Time Alignment Error) is the measure of CCx delay in seconds relative to the reference CC.

Center Freq. is the Frequency Offset plus the measurement channel center frequency for each carrier.

Freq. Offset is the frequency error of the CCx. Except for rounding, this should match the Frequency Error data result on the Summary table (for the reference CC).

Clock Error is the clock error of the CCx. Except for rounding, this should be the same as the Symbol Clock Error data result on the Summary table (for the reference CC).

Cell ID is the cell identifier for the mapped carrier. It is defined in the carrier aggregation table.

See Also

Carrier Aggregation

Matrix Tables