Decoded Info (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
displays the decoded information results for the physical channels with decoding enabled.
Downlink:
Allocation Info - Frequency domain and time domain allocation information:
|
|
Decoded Info:
- PeriodIndex
- BlockIndex
- SymbolIndex
- DecodedBits - Decoded bits by PeriodIndex, BlockIndex and SymbolIndex. If there are more than 100 decoded bits, the decoded bit data will not be displayed in Decoded Info trace. See the Decoded Symbols trace to view decoded data longer than 100 bits.
- CRC Cyclic Redundancy Check - Pass/Fail CRC results by PeriodIndex, BlockIndex and SymbolIndex.
Additional Info:
|
|
Allocation Info - Frequency domain and time domain allocation information:
- PDCCH Index
- CarrierIndex
- BWPIndex
Primary Decoded Info:
- SlotIndex - Index of the decoded slot as configured in the Search Space's Allocated Slots for the selected PDCCH.
- DecodedBits - Decoded bits by SlotIndex. If there are more than 100 decoded bits, the decoded bit data will not be displayed in Decoded Info trace. See the Decoded Symbols trace to view decoded data longer than 100 bits.
- RNTI
- CRC
- Format
- UL Up Link (reverse link: from cell phone to base station)/DL Down Link (forward link: from base station to cell phone)1
- FreqDomainResourceAssignment1
- RBStart1
- RBLength1
- TimeDomainResourceAssignment1
- FreqHop2
- VRBToPRBMapping3
- MCS modulation and coding scheme1
- NewData1
- RedundancyVersion1
- HarqProcessNumber1
- DAI3
- TpcForPUSCH or PUCCH1
- PucchResourceIndicator3
- PDSCHToHarqFeedbackTimingIndicator3
- UL/SUL2
1 Decoded TB for PDCCH Format 0_0 and 1_0
2 Decoded TB for PDCCH Format 0_0
3 Decoded TB for PDCCH Format 1_0
Additional Info:
- AggregationLevel4
- CandidateIndex4
- PayloadSize4
4 Decoded TB with PDCCH Auto Detection selected
Allocation Info - Frequency domain and time domain allocation information:
- PDSCH Physical Downlink Shared Channel Index
- CarrierIndex
- BWPIndex
Primary Decoded Info:
- SlotIndex - Index of the decoded slot as configured in the selected PDSCH's Allocated Slots parameter.
- RV Redundancy Version Index - RV Index as specified in the selected PDSCH's RV Index parameter.
- EffectiveCodeRate - Effective code rate. The effective code rate should be close to the Target Code Rate displayed in the selected PDSCH's Demod Properties.
- CRC - Pass/Fail CRC results by Codeword and SlotIndex.
Additional Info:
- Codeword
- Number Of Code Blocks
- Failed Code Blocks (when PDSCH Auto Detection is selected)
- Number Of Corrected Bits - Number of bits corrected by the error correcting algorithm resulting CRC pass.
Uplink:
Allocation Info - Frequency domain and time domain allocation information:
- PUCCH Index
- CarrierIndex
- BWPIndex
- SlotIndex - Index of the decoded slot as configured in the selected PUCCH's Allocated Slots parameter.
- DecodedBits - Decoded bits by SlotIndex. If there are more than 100 decoded bits, the decoded bit data will not be displayed in Decoded Info trace. See the Decoded Symbols trace to view decoded data longer than 100 bits.
- CRC - Pass/Fail CRC results by SlotIndex.
|
For PUCCH Format 0, decoded bits is provided but it requires the user to provide the payload size information. The CRC is not returned because there is no CRC attached to PUCCH Format 0, so the display shows CRC=***. For PUCCH Formats 1, 2, 3 and 4, when the UCI bit size (PUCCH bit number) is less than 12 bits, there is no CRC result, and the decoded bits are displayed in the Decoded Symbols trace. |
Additional Info:
- SequenceCyclicShift
- OCCIndex
Allocation Info - Frequency domain and time domain allocation information:
- PUSCH Index
- CarrierIndex
- BWPIndex
Primary Decoded Info:
- SlotIndex - Index of the decoded slot as configured in the selected PUSCH's Allocated Slots parameter.
- RV Index - RV Index as specified in the selected PUSCH's RV Index parameter.
- EffectiveCodeRate - Effective code rate. The effective code rate should be close to the Target Code Rate displayed in the selected PUSCH's Demod Properties.
- CRC - Pass/Fail CRC results by Codeword and SlotIndex.
Additional Info:
- Codeword
- Number Of Code Blocks
- Number Of Corrected Bits - Number of bits corrected by the error correcting algorithm resulting CRC pass.
See Also