Pulse Detection Tab (Pulse)

Menu Path: Analysis > Pulse Properties > Pulse Detection

The Pulse Detection tab lets you specify appropriate amplitude reference, threshold and hysteresis levels which are used to derive the Pulse Detection Threshold (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) level as reported in the Pulse Summary results table. The Pulse Detection Threshold (dBm) level is used to detect which measured pulse signal amplitude level transitions will be considered as valid pulses for inclusion within pulse analysis results.

The Pulse Detection Tab allows you to set the following parameters:

See Also

Reference

Threshold (Pulse Detection)

Hysteresis

Ignore Dropouts

Min Pulse Width

Max Pulse Width

Max Pulse Count

Preset Pulse Analysis Measurement