Train Scoring (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis Tab > Train Scoring Panel

In some cases, radar engineers will want to identify and mark the locations of pulse train patterns rather than individual pulses. In this way, they can capture bursts of pulses based on emitter modes, validating figures of merit like pulse width, PRI, etc.

The Analysis tab's Train Scoring panel lets you configure up to four pulse trains of up to 1024 pulses in length. The train scoring algorithm generates a correlation index of the analyzed trains relative to the parameters/metrics configured for each enabled train (Train 1-4). Scoring results are displayed in the Pulse Train Search Table, as opposed to the usual Pulse Table trace. In this table, the correlation is indicated in columns “Train1 Score”, “Train2 Score”, etc. and are scored as a 0 (worst) to 1 (best) range value. Each train is color coded in measurement traces for easy identification (see example below).

Example

The following image displays Pulse Train Search Table results and traces. The train was constructed as follows.

Train 1:

Train 2:

Train 3:

Train 4:

Each train is color coded for easy identification.

See Also

Pulse Table

Pulse Train Search Table

Scoring Metric

Scoring Panel