ASK Auto Bit Rate/Tari (RFID)
Selected (See RFID Standard Setups/Presets Table)
Selecting the checkbox adjusts the expected bit rate (displayed in the and boxes) by analyzing the input data. Clearing the checkbox turns off the adjustment feature and causes the demodulation software to use the values entered and displayed in the and boxes found in the and area of the Format tab.
When the is selected but the algorithm fails to determine the tari or bit rate, the software:
- Displays DATA? on the appropriate traces.
- If average is enabled, excludes the trace from the average.
is ignored when demodulating bursts that use ISO 15693 1-out-of-256 line coding.
See Also