Fwd Bit Rate (RFID)
: 160 kbits/Sec (See RFID Standard Setups/Presets Table)
100 bps to 1 Mbit/Sec
sets the Interrogator-to-Tag bit rate expected by the demodulation software.
Selecting the checkbox allows the measurement software to adjust the expected bit rate (displayed in the and boxes) by analyzing the input data. Clearing the checkbox turns off the automatic adjustment feature and causes the demodulation software to use the values entered and displayed in the and boxes.
The value in the box sets the bit rate used by the RFID demodulation software. The bit rate value is specified (rather than the symbol rate) because the symbol rate can vary depending on the modulation scheme.
The area (beneath the and boxes) displays the approximate symbol rate defined by the protocol, the format, and the or setting.
When is selected as the RFID standard and is set to either or , is automatically set as follows:
- : Fwd Bit Rate set to 26.484375 kbps
- : Fwd Bit Rate set to 1.6552734375 kbps
See Also
Format Tab (RFID Demod Properties)