Tari (RFID)
6.25 uSec (See RFID Standard Setups/Presets Table)
100 nSec to Acquisition Length / 2
sets the tari rate for the Interrogator expected by the demodulation software.
Selecting the checkbox adjusts the expected bit rate (displayed in the and boxes) by analyzing the input data. Clearing the checkbox turns off the adjustment feature and causes the demodulation software to use the values entered and displayed in the and boxes.
The value in the box is the time (in seconds) required when using PIE line encoding. The value is set by time because the bit rate varies depending on the data value encoded.
The area (beneath the and boxes) displays the approximate symbol rate defined by the protocol, the format, and the or setting.
See Also