CW Analysis (RFID)
: Cleared (See RFID Standard Setups/Presets Table)
When mode is selected, the CW Summary Table and pre-demod traces are available. All other results are labeled "DATA?"
In this mode averaging is rejected if no CW power-on and CW power-off are found in the data.
To ensure the rising edge of the CW signal is properly detected, use an appropriate amount of pre-trigger.
See Also
Format Tab (RFID Demod Properties)