Modulation Analysis (RFID)
: Selected (See RFID Standard Setups/Presets Table)
Selecting the button directs the RFID demodulation software to examine and demodulate a burst from within the acquired signal. In this mode, the demodulation software produces signal quality metrics like modulation depth and ASK Error Time. This measurement requires only that at least one complete burst is present in the acquired data.
When mode is enabled, all results are computed except the CW Summary table. The table is labeled with a "DATA?" trace. When no burst is found in the data, averaging is not performed.
See Also