Ret Bit Rate (RFID)
40 kBits/Sec (See RFID Standard Setups/Presets Table)
100 bps to 1 Mbits/Sec
The parameter sets the Tag-to-Interrogator bit rate expected by the demodulation software.
Selecting the checkbox allows the measurement software to adjust the expected bit rate (displayed in the and boxes) by analyzing the input data. Clearing the checkbox turns off the automatic adjustment feature and causes the demodulation software to use the values entered and displayed in the and boxes.
The value in the text box sets the bit rate used by the RFID demodulation software. The bit rate value is specified (rather than the symbol rate) because the symbol rate can vary depending on the modulation scheme.
The area (beneath the and boxes) displays the approximate symbol rate defined by the protocol, the format, and the or setting.
See Also