Sync Search Tab (RFID)
The tab of the synchronizes the demodulation software to a predefined protocol pattern or to a bit pattern that is specified. These values are set to previously defined values when the Preset to Standard button on the Format Tab is used.
The parameters controlled on the tab include:
See Also
Format Tab (RFID Demod Properties)
Filter Tab (RFID Demod Properties)
Time Tab (RFID Demod Properties)
Advanced Tab (RFID Demod Properties)
RFID Demod Properties Dialog Box