Time Tab (RFID)
The tab of the specify the signal capture configuration parameters. These values are set to previously defined values when the Preset to Standard button on the Format Tab is used.
The Time tab dialog box configures these parameters:
See Also
Format Tab (RFID Dempd Properties)
Filter Tab (RFID Dempd Properties)
Sync Search Tab (RFID Dempd Properties)