ASK Err (RFID)
Menu Path:
ASK Err (error) is calculated as a percentage from Demod and Demod .
The ASK Err (error) shows the rms average of Demod Error Time. It is computed at the symbol points. Points between symbols are not used to compute the ASK Err.
The ASK Err measurement is the ASK equivalent of the BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros. measurement EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format..
See Also