Ref Time (RFID)
The trace is the reference of ASK signal which is shaped using . The default display format of this trace is Real.
Because this trace is a real value trace normalized by (A-B), the minimum value is near 0 and the maximum is near 1 (100%), identically to .
The trace title is determined by the type of modulation format specified by the Fwd Format or the Ret Format selected on the Format Tab (RFID). If the modulation format specified is , the trace title will read ; if is selected, the trace title will read .
See Also