Error Time (RFID)
Thetrace is calculated by [Meas Time] – [Ref Time]. The default display format of this trace is Real.
The trace title is determined by the type of modulation format specified by the Fwd Format or the Ret Format selected on the Format Tab of the dialog box. If the modulation format specified is , the trace title will read ; if is selected, the trace title will read .
See Also
Selecting the RFID Demodulator