Summary (RFID)
The Demod table displays the results of the RFID software's demodulation analysis. The information presented in the trace table depends on the type of modulation format specified by the Fwd Format or the Ret Format selection on the Format tab on the dialog box and on the direction of the burst specified by the Burst Search parameters.
The trace title is determined by the type of modulation format specified by the Fwd Format or the Ret Format selected on the of the dialog box. If the modulation format specified is , the trace title will read ; if is selected, the trace title will read .
See Also