Auto-detect for all code channels (TD-SCDMA)
Selected (See TD-SCDMA Standard Setups/Presets Table.)
mode tests all code channels for SF1 and SF16 for modulation formats QPSK Quadrature phase shift keying and 16QAM, then performs analysis based on the detected modulation format.
is only available when Enable HSPA/8PSK is selected.
The can be selected from a drop-down list that includes Auto, QPSK, 8PSK, 16QAM, and 64QAM for SF1 and SF16. QPSK is the only option available for SF2, SF4, and SF8 (in compliance with the TD-SCDMA standard).
See Also