Result Length (W-CDMA(3GPP)/HSPA)
15 Slots (See W-CDMA(3GPP) Standard Setups/Presets Table.)
: 1 to 64
specifies the signal capture length in terms of slots or equivalent slot time. This is the number of slots available for data analysis. The actual analysis interval is determined by Measurement Offset and Measurement Interval properties which must be specified to be within the , such that >= 0 and + <= . Make sure that the is long enough to capture all the desired data.
may be entered as an integer number of slots, frames or time. Choose to use seconds and the VSA will automatically increment the time as necessary to obtain an integer number of slots.
Slot: one slot is equal to 2560 chips (666.7 µs at the default chip rate) and one frame is equal to 15 slots (10 ms at the default chip rate).
is a primary factor determining measurement speed. Smaller increases measurement speed but a less than 6 Slots may cause inaccurate measurement results.
For more information, see About Measurement Interval and Offset.
See Also
About Measurement Interval and Offset