AM/FM Metrics (Option 355) Commands - Requires SA


In this topic:

- Metrics

See Also

- Commands that are Common to All Modes

- Correction Methods Explained

- New Programming Commands

- Status Registers

Metrics

Set the AM/FM Metrics measurement type (Select 1 of n measurement choices)

[:SENSe]:MEASurement:ADEMod

Set the AM demodulation window's Y axis--top amplitude

[:SENSe]:ADEMod:METRics:AMTY    

 Select type of metrics AM FW wideband or narrow band

[:SENSe]:ADEMod:METRics:DTYPe 

Set the FM demodulation window's Y axis--top amplitude

[:SENSe]:ADEMod:METRics:FMTY 

Enables/disables the Audio ON or OFF while metrics enabled

[:SENSe]:ADEMod:METRics:LON   

Sets the Listen time for the measurement

[:SENSe]:ADEMod:METRics:LTIMe   

Enable display of Peak+ and Peak – in the demodulation window

[:SENSe]:ADEMod:METRics:MMENable  

Sets the time span of the demodulation window

[:SENSe]:ADEMod:METRics:STIMe

Sets the Tune (Center) frequency

[:SENSe]:ADEMod:METRics:TFReq  

Returns 8 doubles of the AM measurement  (query only)

:DISPlay:ADEMod:METRics:AM:RESults:DATA?

Returns 8 doubles of the FM measurement  (query only)

:DISPlay:ADEMod:METRics:FM:RESults:DATA?