:DLOGging:FILE:FOLDer <char>

(Read-Write) Sets the log file save/recall folder where the log files are save/recalled (CS | PAA | OTA).

See also, DLOG:FILE:ASAVe, DLOG:FILE:TYPE, DLOG:REC:STAR, MMEMory:LOAD:DLOG, and MMEM:STOR:DLOG

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA

Parameters

 

<character>

File storage folder. Choose from:

DEFault- The default folder for the current mode (UserData\RecordPlayback\Mode, where Mode is initialized for the current mode)

  • Channel Scanner = "CS"

  • Phased Array Antenna = "PAA"

  • Over-the-Air = "OTA"

SYSTem – The current system folder (determined by the general Save/Recall settings)

Examples

DLOG:FILE:FOLD SYST */Sets the current system folder that has previously set in the Save/Recall settings

DLOG:FILE:FOLD DEF  */This is the preset condition that uses the current mode's folder as the folder to save/recall log files)

Query Syntax

DLOG:FILE:FOLD?

Default

DEF


Last Modified:

01dec2020

New command (12.1x)