:MMEMory:LOAD:DLOG  <string>

(Write-only) Load a *.csv or *.kml or *.drec log file (i.e., *.drec files are only applicable for PAA mode).

See also, DLOG:FILE:ASAVe, DLOG:FILE:TYPE, DLOG:REC:STAR, MMEMory:STOR:DLOG, and DLOG:FILE:FOLDSee more MMEMory commands.

See more MMEMory commands.

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA

Parameters

 

<string>

For *.csv files, provide filename and .csv extension.

For *.kml files, provide filename and .kml extension.

For *.drec files, provide filename and .drec extension

<char>

Memory device where the Antenna file is stored. Choose from the following:

  • INTernal - internal storage device

  • USB - first USB device

  • SD - SD storage card

Examples

MMEM:LOAD:DLOG "MyAntenna",INT

mmemory:load:dlog antenna "demo_antenna_26m_3g.kml",internal

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01dec2020

Added new topic/commands (A12.1x)

01june2019

New command