(Read-Write) Saves a CSV or KML or DCAT (DCAT is applicable to PAA mode only) file to a compatible mode's folder on customer-selected device: Int, USB, SD card. See also, DLOG:FILE:ASAVe, DLOG:FILE:TYPE, DLOG:REC:STAR, MMEMory:LOAD:DLOG, and DLOG:FILE:FOLD See more MMEMory commands. |
|
Relevant Modes |
Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA |
Parameters |
|
<filename> |
|
Examples |
:DLOGging:STORe:DLOG 'samplefileKML' */Stores a KML samplefile :DLOGging:STORe:DLOG 'samplefileCSV' */Stores a CSV samplefile :DLOGging:STORe:DLOG 'samplefileDCAT' */Stores a DCAT samplefile - (PAA mode only) |
Query Syntax |
:DLOGging:FILE:MMEMory:STORe:DLOG? 'samplefile' |
Return Type |
character |
Default |
n/a |
Last Modified:
01dec2020 |
Added new topic/commands (A12.1x) |