SYSTem:HEAD:CORRections:ASETup  <bool>

(Read-Write) Set and query the frequency converter corrections setup state (Auto  Setup = ON (1) / Edit SA = OFF(0)).

See also, SYST:HEAD:CORR.

Relevant Modes

5G NR, 5G NR EVM Conducted, 5G TF, EMI, IQA, LTE FDD, PAA, RTSA, SA

Parameters

 

<bool>

Frequency converter correction state. Choose from:

OFF (or 0) - Edit SA is enabled. In SA mode a converter correction file can be edited/created.

ON (or 1) - Converter correction ON. A default (rough) frequency converter correction file is automatically recalled.

Note: Unless otherwise specified, on the FieldFox, *.csv files are initially stored and recalled by default from the "[INTERNAL]:\Converter" folder.

Examples

SYST:HEAD:CORR:ASET 1 'Enables the default frequency converter corrections.

Query Syntax

SYSTem:HEAD:CORRections:ASETup?

Return Type

Boolean

Default

ON(1)


Last Modified:

04no2022

Added EMI mode (12.3x)

20apr2020

New command A.12.00