(Read-Write) Set and query the align all (InstAlign all) state. When the individual alignments are coupled (Align All state is set to Auto), the state of all of them can be changed simultaneously using the Align All (i.e., InstAlign Amplitude Alignment, RF Burst, and Channel Equalization alignments). Refer to ALIGn:ALL:NOW. |
|
Relevant Modes |
ChScn, EMI, IQA, LTE FDD, 5G NR, 5G NR EVM Conducted, PAA, SA, CPM, RTSA All models with InstAlign capability (All EXCEPT N9912A). |
Parameters |
|
<character> |
InstAlign state. Choose from: AUTO - The alignment process is performed every 300 seconds or when the temperature has changed about 1 degree. It occurs only at the beginning of a sweep and takes about 0.5 seconds to complete. HOLD - The alignment process is stopped, but the last alignment values are applied to subsequent sweeps. OFF - The alignment process is NOT performed. Only factory correction values are used. |
Examples |
ALIG:AMPL HOLD |
Query Syntax |
[:SENSe]:ALIGnment:ALL[:STATe]? |
Return Type |
Character |
Default |
AUTO |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
10dec2019 |
Added 5G NR, 5G NR EVM Conducted, and PAA (11.5x) |
20june2019 |
New command |