(Write-Only) Sets the Cal Method to QuickCal - Enhanced Response. Calibrates either forward (S11/S21) or reverse (S22/S12) measurements. This Cal Method requires mating (insertable) DUT connectors. Use [:SENSe]:CORRection:COLLect:CONNector to change connector and gender. Requires QuickCal Option.
Note: QuickCal commands do not apply to N995x/6xA or B model FieldFoxes. |
|
Relevant Modes |
N9912A with Opt 110: CAT, NA - ONLY <1,2> are supported (NOT 2,1 reverse) All other models with Full S-parameter option, CAT, NA modes. To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
Parameters |
|
<p1> |
First port.
|
<p2> |
Second port to calibrate.
|
Examples |
CORR:COLL:METH:QCAL:ERES 1,2 |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
02apr2019 |
Added B model content |
18-Oct-2012 |
Added new models |