(Read-Write) Set and query the DUT uncertainty setup values being measured. See also [:SENSe]:CORRection:DUT:INGamma, [:SENSe]:CORRection:DUT:OUTGamma, [:SENSe]:CORRection:DUT:SPEC, [:SENSe]:CORRection:DUT:DISTribution. See also, MMEMory:LOAD:DUT and MMEMory:STORe:DUT. |
|
Relevant Modes |
|
Parameters |
|
<character> |
DUT mode uncertainty settings. Choose from: SPOT- Sets the DUT mode to Spot, where you can customize the DUT uncertainty values. TABL - Time per point can be set, but other integration SCPIs are not settable. |
Examples |
CORR:DUT:MOD SPOT CORR:DUT:MOD TABL |
Query Syntax |
CORRection:DUT:MODe? |
Return Type |
Character |
Default |
SPOT |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |