[:SENSe]:CORRection:DUT:SPOT:DISTribution

(Read-Write) Set and query the DUT specified fixed value. This value indicates the nature of the entered value relative to the population of values it represents. (i.e., Fixed, Rayleigh, or Uniform (Uniform in Circle).

Note: Only available when CORR:DUT:MOD is set to SPOT.

See also [:SENSe]:CORRection:DUT:MODe, [:SENSe]:CORRection:DUT:SPOT:INGamma, [:SENSe]:CORRection:DUT:SPOT:OUTGamma, [:SENSe]:CORRection:DUT:SPOT:SPECify.

See also, MMEMory:LOAD:SPOT:DUT and MMEMory:STORe:SPOT:DUT.

Relevant Modes

 NF

Parameters

 

<character>

DUT Spot mode's distribution value. Choose from:

RAYL - The probability density function (pdf) of the magnitude of the reflection coefficient is a Rayleigh distribution. This is normally the case for specified values when the overall mismatch is due to several interacting impedance transitions within the device.

UNIF - A distribution that was historically used in the industry, before the Rayleigh research, as documented in Keysight Application Note 1449-3, but is rarely accurate. Refer to https://literature.cdn.keysight.com/litweb/pdf/5988-9215EN.pdf.

FIX - The reflection coefficient magnitude is always at the given level. This is often the case when measured values are used.

Examples

CORR:DUT:SPOT:DIST FIX

CORR:DUT:SPOT:DIST RAYL

Query Syntax

CORRection:DUT:SPOT:DIST?

Return Type

Character

Default

FIX


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)