[:SENSe]:CORRection:DUT:SPOT:SPECify

(Read-Write) Set and query the DUT specified fixed value. This value indicates the nature of the entered value relative to the population of values it represents.

Note: Only available when CORR:DUT:MOD is set to SPOT.

See also [:SENSe]:CORRection:DUT:MODe, [:SENSe]:CORRection:DUT:ISPOT:INGamma, [:SENSe]:CORRection:DUT:SPOT:OUTGamma, [:SENSe]:CORRection:DUT:SPOT:DISTribution.

See also, MMEMory:LOAD:DUT and MMEMory:STORe:DUT.

Relevant Modes

 NF

Parameters

 

<character>

DUT Spot mode's fixed value. Choose from:

MAX - Use this if this value represents the largest possible reflection coefficient for the population of devices to which the DUT belongs. This is true for "does not exceed" specifications.

PCTL95 - Use this if 95% of the population has a lower reflection coefficient than the value entered. This is the case for "2 standard deviation" (2s) type specifications.

PCTL80 - Use this if 80% of the population has a lower reflection coefficient than the value entered.

MED or MEAN - Use this if this value represents the median / mean reflection coefficient for the population of devices to which the DUT belongs.

FIX - Use this if the value is a measured value for the DUT.

Examples

CORR:DUT:SPOT:SPEC PCTL95

CORR:DUT:SPOT:SPEC MED

Query Syntax

CORRection:DUT:SPOT:SPEC?

Return Type

Character

Default

FIX


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)