[:SENSe]:CORRection:UNCertainty:CALibration <bool>

(Read-Write) Set and query the user calibration uncertainty ON | OFF state.

See also, [:SENSe]:CORRection:UNCertainty:JITTer, [:SENSe]:CORRection:UNCertainty:MISMatch, [:SENSe]:CORRection:UNCertainty:ENR, [:SENSe]:CORRection:UNCertainty:COVerage, and [:SENSe]:CORRection:UNCertainty:BARS

For trace-related uncertainty commands, refer to CALCulate:[SELected]TRACe:UNCertainty:DATA?, CALCulate:[SELected]:TRACe:UNCertainty:UPPer:DATA?, and CALCulate:[SELected]:TRACe:UNCertainty:LOWer:DATA?.

Relevant Modes

NF

Parameters

 

<bool>

User calibration uncertainty state. Choose from:

0 or OFF - User calibration uncertainty OFF

1 or ON - User calibration uncertainty ON

Examples

CORR:UNC:CALC ON 'Can only be enabled when a user calibration has been completed

Query Syntax

[:SENSe]:CORRection:UNCertainty:CALibration?

Return Type

Boolean

Default

Off (0)


Last Modified:

18-Oct-2012

Edited for new models