[:SENSe]:CORRection:UNCertainty:COVerage <char>

(Read-Write) Set and query the value of the current settings uncertainty contributions coverage (1σ, 2σ, or 3σ).

See also, [:SENSe]:CORRection:UNCertainty:JITTer, [:SENSe]:CORRection:UNCertainty:MISMatch, [:SENSe]:CORRection:UNCertainty:ENR, [:SENSe]:CORRection:UNCertainty:CALibration, and [:SENSe]:CORRection:UNCertainty:BARS

For trace-related uncertainty commands, refer to CALCulate:[SELected]TRACe:UNCertainty:DATA?, CALCulate:[SELected]:TRACe:UNCertainty:UPPer:DATA?, and CALCulate:[SELected]:TRACe:UNCertainty:LOWer:DATA?.

Relevant Modes

 NF

Parameters

 

<character>

Current settings uncertainty coverage value. Choose from:

SD1 - 1σ (About 68% of the values fall within 1 standard deviation of the mean.)

SD2 - 2σ (About 95% of the values fall within 2 standard deviations of the mean.)

SD3 - 3σ (About 99.7% of the values fall within 3 standard deviations of the mean.)

Examples

CORR:UNC:COV SD1

CORR:UNC:COV SD3

Query Syntax

CORRection:UNC:COV?

Return Type

Character

Default

SD2


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)