[:SENSe]:CORRection:UNCertainty:ENR<bool>

(Read-Write) Set and query the ENR source uncertainty ON | OFF state.

See also, [:SENSe]:CORRection:UNCertainty:JITTer, [:SENSe]:CORRection:UNCertainty:MISMatch, [:SENSe]:CORRection:UNCertainty:CALibration, [:SENSe]:CORRection:UNCertainty:COVerage, and [:SENSe]:CORRection:UNCertainty:BARS

For trace-related uncertainty commands, refer to CALCulate:[SELected]TRACe:UNCertainty:DATA?, CALCulate:[SELected]:TRACe:UNCertainty:UPPer:DATA?, and CALCulate:[SELected]:TRACe:UNCertainty:LOWer:DATA?.

Relevant Modes

NF

Parameters

 

<bool>

ENR source uncertainty state. Choose from:

0 or OFF - Source uncertainty OFF

1 or ON - Source uncertainty ON

Examples

CORR:UNC:ENR 0

Query Syntax

[:SENSe]:CORRection:UNCertainty:ENR?

Return Type

Boolean

Default

On (1)


Last Modified:

18-Oct-2012

Edited for new models