(Read-Write) Set and query the frequency span of the trace. |
|
Relevant Modes |
CAT, EMI, NA, NF, SA, CPM, RTSA CPM Mode: Limited to between 10 Hz and 100 MHz. SPAN is equivalent to the “channel power integration bandwidth”. |
Parameters |
|
<num> |
Frequency span in Hz. Choose a number between the maximum MINUS the minimum frequency of the FieldFox. This command will accept MIN and MAX as arguments.
|
Examples |
FREQ:SPAN 10E6 FREQ:SPAN MIN |
Query Syntax |
[:SENSe]:FREQuency:SPAN? |
Return Type |
Numeric |
Default |
Maximum MINUS minimum frequency range of the FieldFox. |
Last Modified:
01-june-2018 |
Added NF mode (10.30) |
10-june-2016 |
Added RTSA mode (9.50) |
1-April-2014 |
Added CPM |