(Read-Write) Set and query the Auto RF Attenuation state. See also :POW:ATT. |
|
Relevant Modes |
5GTF, 5G NR, 5G NR EVM Conducted, EMI, PAA, SA, LTE FDD, RTSA, IQA |
Parameters |
|
<boolean> |
Auto RF Attenuation state. Choose from: O or OFF - RF Attenuation is set manually 1 or ON - RF Attenuation is set automatically |
Examples |
POW:ATT:AUTO 1 |
Query Syntax |
[:SENSe]:POWer[:RF]:ATTenuation:AUTO? |
Return Type |
Boolean |
Default |
ON |
Last Modified:
31oct2019 |
Added PAA mode |
03dec2018 |
Added LTE FDD & 5GTF (A.11.0) |
22oct2017 |
Added IQA mode (10.1x) |
10-june-2016 |
Added RTSA mode (9.50) |