[:SENSe]:INTegration:MODe <char>

(Read-Write) Set and query the Integration mode setting.

See also [:SENSe]:INTegration:JITTer, [:SENSe]:INTegration:MAXTime, [:SENSe]:INTegration:WARNing, and [:SENSe]:INTegration:TIMe.

Relevant Modes

 NF

Parameters

 

<character>

Integration mode. Choose from:

AUTO -  The FieldFox Noise Figure application chooses the optimum integration time for each of the noise power measurements needed (i.e., noise source on, noise source off, and receiver reference) to compute the device's noise figure with the selected amount of measurement jitter in the shortest possible time.  

FIXED -  Time per point can be set, but other integration SCPIs are not settable.

Examples

INT:MOD FIXED

Query Syntax

INTegration:MODe?

Return Type

Character

Default

AUTO


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)