[:SENSe]:INTegration:TIMe <num>

(Read-Write) Set and query the Integration mode's time per point setting (Time/Pt) setting. Use this command when [:SENSe]:INTegration:MODe = FIXED.

See also [:SENSe]:INTegration:MODe, [:SENSe]:INTegration:JITTER, [:SENSe]:INTegration:WARNing, and [:SENSe]:INTegration:MAXTime.

Relevant Modes

 NF

Parameters

 

<numeric>

Time per point. Choose from:

Varies, because the setting is coupled to other settings

Examples

INT:TIM 0.04

Query Syntax

INTegration:TIMe?

Return Type

Numeric

Default

5.0E-01


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)