[:SENSe]:INTegration:WARNing <bool>

(Read-Write) Set and query the Integration mode's jitter warning (Jitter Warning). Enables and disables the jitter warning when [:SENSe]:INTegration:MODe = AUTO.

See also [:SENSe]:INTegration:MODe, [:SENSe]:INTegration:JITTER, [:SENSe]:INTegration:MAXTime, and [:SENSe]:INTegration:TIMe.

Relevant Modes

 NF

Parameters

 

<boolean>

Integration warning per point. Choose from:

ON(1) - Enables the jitter warning.

OFF(0) - Disables the jitter warning.

Examples

INT:WARN 1

Query Syntax

INTegration:WARNing?

Return Type

Boolean

Default

1


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)