|
Note: This command was previously named [:SENSe]:ISOurce:FREQuency[:CW]. That syntax will still work, but the new syntax should be used for new development. (Read-Write) Set and query the Independent Source CW frequency. Use SOURce:MODE to set Independent Source to CW mode. Use SOURce:ENABle to enable Independent Source. |
|
|
Relevant Modes |
EMI, SA, Pulse Generator |
|
Parameters |
|
|
<num> |
CW frequency. Choose a value within the IQA and SA mode frequency range. |
|
Examples |
SOUR:FREQ 1e9 |
|
Query Syntax |
SOURce:FREQuency[:CW]? |
|
Return Type |
Numeric |
|
Default |
IQA, SA mode center frequency |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
25-Mar-2014 |
Name change |
|
10-Oct-2010 |
New command (5.30) |