|
Note: (Read-Write) Set and query the Independent Source mode setting. Use SOURce:ENABle to enable Independent Source. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Independent source mode. Choose from: CW - The internal source is set to CW. Use SOURce:FREQuency[:CW] to set the frequency. TCW - The internal source is set to tracking CW. SRTS - “Stimulus Response Tracking Sweep". The internal source tracks with the SA receiver. Use SOURce:NORMalize to normalize the trace. |
|
Examples |
SOUR:MODE CW |
|
Query Syntax |
SOURce:MODE? |
|
Return Type |
Character |
|
Default |
CW |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
25-Mar-2014 |
Name change |
|
10-Oct-2010 |
New command (5.30) |