SYSTem:ANTenna:EMF:TYPe <string>

(Read-Write) Set and query the EMF (USB) antenna type.

NOTE: This command supersedes SYSTem:ANTenna:USB:TYPe. To learn more, refer to Replacement Commands topic.

Relevant Modes

SA, 5G EVM, EMI, EMF Antenna, Pulse Generator

Parameters

 

<string>

EMF Antenna Type value. Choose from:

Manual – Sets the EMF antenna to manual when physically moving the antenna for manual  adjustment..

ARIA6000 – Sets the EMF antenna-type to be triaxial.

Note: Only one USB triaxial antenna is compatible with the FieldFox.

FSH3D – Sets the EMF antenna-type to be FSH3D

Examples

SYST:ANT:EMF:TYP "Manual" */Selects the EMF antenna-type to Manual.

SYST:ANT:EMF:TYP "ARIA6000" */Selects the EMF antenna-type to ARIA6000.

SYST:ANT:EMF:TYP "FSH3D" */Selects the EMF antenna-type to FSH3D.

Query Syntax

SYST:ANT:EMF:TYP?

Return Type

string

Default

Manual


Last Modified:

06mar2024

Added new compatible command for EMF mode (A.13.00)