|
(Read-Write) Set and query the Display Units, regardless of the current Scale setting. The UNIT choice affects the following: Reference Level, Trigger Level, Limit Lines, Marker annotation, Channel Power, and Adjacent Channel Power. This command affects the TRACe:DATA? return values. Antenna correction units are available ONLY by loading an Antenna file that contains the desired units setting. Use MMEMory:LOAD:ANTenna. |
|
|
Relevant Modes |
Channel Scanner, EMI, PAA, SA,CPM |
|
Parameters |
|
|
<char> |
Display Units with Antenna correction OFF, choose from:
Standard Units: The following are NF and SA ONLY - not allowed for CPM
Field Strength Units: The following are CS and SA ONLY - not allowed for CPM
|
|
Examples |
AMPL:UNIT W |
|
Query Syntax |
[:SENSe]:AMPLitude:UNIT? |
|
Return Type |
Character |
|
Default |
DBM |
Last Modified:
|
04nov2022 |
Added EMI mode (12.3x) |
|
01june2018 |
Added Channel Scanner (ChScn) - (10.3) |
|
24-Mar-2014 |
Added CPM |
|
20-Oct-2010 |
New command (5.30) |