Read-only |
About Cal Sets |
Description |
Returns error term data from the Cal Set by specifying the string name of the error term.
|
VB Syntax |
pdata = calset.GetErrorTermByString(setNumber, errorTerm) |
Variable |
(Type) - Description |
|
pdata |
(Variant) Two-dimensional safe array to store the returned data. Memory for the returned Variant is allocated by the PNA and must be released by client. Note: See also getErrorTermComplexByString on the ICalData3 interface to avoid using the variant data type. |
|
calset |
A Cal Set (object) |
|
setNumber |
(Long) Set number of the required Cal Set data. See GetCalSetUsageInfo to determine the setNumber.
New beginning PNA Rev 7.2: The channel error term data contains interpolation, fixturing, and port extension data if each is ON.
|
|
errorTerm |
(String) The string name used to identify a particular error term in the Cal Set. An example string for port 3 directivity in a full 2 port cal might be "Directivity(3,3)". To determine the string names of error terms, see GetErrorTermList2. |
Return Type |
Variant |
Default |
Not Applicable |
Examples |
|
C++ Syntax |
HRESULT GetErrorTermByString (long SetNumber, BSTR bufferName, VARIANT* pdata); |
Interface |
ICalSet2 |