Description |
Initializes a cable repeatability characterization for the specified channel and port. |
VB Syntax |
UncertChar.InitiateCableCharacterization (chan, port,iterations) |
Variable |
(Type) - Description |
|
UncertChar |
A Characterizer (object) |
chan |
(Long) Channel number to calibrate. Note: chan MUST be the active channel. |
port |
(Long) Port number to use in the characterization. |
iterations |
(Long) Number of Iterative connections of the standards to be measured for the characterization. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
oUncerChar.InitiateCableCharacterization(2,2,20) |
C++ Syntax |
HRESULT InitiateCableCharacterization([in] long channel, [in] long portNum, [in] long numIterationsPerStep, [out,retval] long* pNumSteps); |
Interface |
IUncertaintyCharacterizer |
The following existing commands on the GuidedCal object are used to perform the initialized cable repeatability characterization:
MinimumIterationsForStep Property
IterationCountForStep Property
Last Modified:
|
28-Oct-2014 |
New topic |