Write/Read |
About SMC Phase |
Description |
Set and return the method of setting the delay through the calibration mixer. To select Phase Reference Cal method for correcting an SMC+Phase measurement, use ImportDataSet Method. |
VB Syntax |
smc.DelayCalculationMethod = value |
Variable |
(Type) - Description |
|
smc |
An SMCType (object) |
|
value |
(Enum as NADelayCalculationMethod) 0 - naDelayCalculationMethod_FixedDelay - use a known delay value set with FixedDelay Property 1 - naDelayCalculationMethod_MixerCharacterizationFile - use the S2P file set with MixerCharacterizationFile Property |
Return Type |
Enum |
Default |
0 - naDelayCalculationMethod_FixedDelay |
Example |
SMC.DelayCalculationMethod = naDelayCalculationMethod_FixedDelay |
C++ Syntax |
HRESULT put_DelayCalculationMethod(tagNADelayCalculationMethod Value); HRESULT get_DelayCalculationMethod(tagNADelayCalculationMethod* Value); |
Interface |
SMCType5 |
Last Modified:
|
25-Mar-2010 |
MX New topic |