Write/Read |
About PNA-X Pulsed Capabilities |
Description |
Sets and returns whether the PNA configures the 3-stage digital filter settings or they will be configured manually. When making manual settings, also send ADCCaptureMode Property which routes the IF through the 3-stage filter. |
VB Syntax |
spm4.FilterMode = value |
Variable |
(Type) - Description |
|
spm4 |
A SignalProcessingModuleFour (object) |
|
value |
(enum as NAModes) Filter mode. Choose from: naAUTO PNA controls digital filter settings. naMANUAL You control digital filter settings using other SignalProcessingModuleFour commands. |
Return Type |
Enum |
Default |
naAUTO |
Examples |
spm4.FilterMode = naAUTO 'Write |
|
mode = spm4.FilterMode 'Read |
|
C++ Syntax |
HRESULT get_FilterMode(tagNAModes* dspMode); HRESULT put_FilterMode(tagNAModes dspMode); |
Interface |
ISignalProcessingModuleFour |