Write/Read |
About PNA-X Pulsed Capabilities |
Description |
Sets and returns the ADC capture mode modeled as a 2-pole switch in the diagram on the SignalProcessingModuleFour page. The switch either bypasses or routes the IF through the 3-stage digital filter. |
VB Syntax |
spm4.ADCCaptureMode = value |
Variable |
(Type) - Description |
|
spm4 |
A SignalProcessingModuleFour (object) |
|
value |
(Enum as NAStates) Capture mode. naOFF (0) - The digital filters are used to process IF information. The filters can be configured automatically or manually using FilterMode Property. naON (1) - The digital filters are bypassed and the raw ADC readings are taken directly. With DSP 4 versions, a maximum of 4096 data points per sweep can be acquired. With DSP 5 versions, the PNA maximum data points per sweep can be acquired. |
Return Type |
Enum |
Default |
OFF |
Examples |
spm4.ADCCaptureMode = 0 'Write |
|
mode = spm4.ADCCaptureMode 'Read |
|
C++ Syntax |
HRESULT get_ADCCaptureMode(tagNAStates* pCaptureMode); HRESULT put_ADCCaptureMode(tagNAStates pCaptureMode); |
Interface |
ISignalProcessingModuleFour |
Last Modified:
|
26-Aug-2010 |
Updated for DSP 5 (A.09.30) |
|
18-Jun-2007 |
MX New topic |