Read/Write

PassFailScope Property


Description

Sets and reads the Scope of the PassFail line on the HANDLER IO connector (pin 33).  Learn more about Global Pass/Fail.

 VB Syntax

object.PassFailScope = value

Variable

(Type) - Description

object

(object) - An Aux I/O or Handler IO object

value

(enum NAPassFailScope ) Choose from:

0 - naChannelScope - The PassFail line returns to its default state before sweeps on the next channel start.  (A channel measurement may require several sweeps.)

1 - naGlobalScope - The PassFail line returns to its default state before the sweeps for the next triggerable channel start.

The default state of the PassFail line before a measurement occurs and after a failure occurs is set by the PassFailMode property.

Return Type

enum NAPassFailScope

Default

1 - naGlobalScope

Examples

HWAuxIO.PassFailScope = naGlobalScope 'Write

scope = HWAuxIO.PassFailScope 'Read

C++ Syntax

HRESULT put_PassFailScope ( tagNAPassFailScope Scope );

HRESULT get_PassFailScope ( tagNAPassFailScope* Scope );

Interface

IHWAuxIO

IHWMaterialHandlerIO